Editor
In this topic, Editor related FAQs are listed.
How can I quickly open declaration of any variable, function name, macro, or header file from within Editor?
How can I open definition of a function or header file from within the editor?
If I am using a Macintosh computer, what is the alternate to using the F3 key in Editor to open declarations?
How can I change the color that highlights the current line in a source code file?
Is it possible to view definition of a macro or a variable in the source code file?
Can the CodeWarrior IDE assist me in writing the source code?
How can I change the tab width/size?
Is it possible to display line numbers in Editor?
Is it possible to change the default code format settings?
How can I quickly switch to a header file from within the source code file?
How does the CodeWarrior IDE differentiate between enabled and disabled macros?
How can I configure predefined macros in the CodeWarrior IDE?
Is it possible to view evaluated expansion of a macro in the CodeWarrior IDE?
Is it possible to roll back the changes I did to my source code?
Is there a way to change the default color of comments that span across multiple lines?
Is there a way to revert to the original contents of a source code file?
How do I convert Line Delimiters to the Unix format?
Why do I get the following error message when I try to edit a source code file?
What does an asterisk on the Editor title bar mean?
How can I find out where a function is declared in my source code?
How can I open .tcl extension files in the Editor window?
Is it possible to condense a large source file by folding/unfolding different portions of code?
How can I generate S19, Intel Hex, and Binary files for my project?
How can I use the Burner for the Kinetis derivatives?
I have created two build configurations one for debug and another for release. How can I specify a burner bbl file for each build configuration?
Is there a way to determine in which workspace I am working currently?
How can I share same installation of the CodeWarrior software with multiple users?
How can I comment/uncomment a block of code in the editor?
How can I compare files in CodeWarrior IDE?
Is there a way to compare files that are not in project?
How do I switch between the source files in the Editor view?
I want to edit my source files, but all the other views are using the space as well. How do I maximize the editor view to have better working area?
How do I remove blank lines in the Editor view?