What Bootloader Shell commands I can use?You can use the following bootloader shell commands:
CLS1 help | status
This command prints help or status information.
BL help
This command prints help information.
BL status
This command shows the application flash range, and the content of the application vector table.
BL erase
This command erases the application flash blocks.
BL restart
This command restarts the user application (if any) with jump to the reset vector.
BL load s19
This command loads the S19 file.