Use Pre-Defined Programming Task

To use a pre-defined flash programming task, you first import its *.xml file into the Target Tasks view. CodeWarrior for Microcontrollers provides default flash configuration files for a wide variety of supported target boards.

The pre-defined task files are in the following directories.

Table 1. Pre-defined Task Files Locations
Connection Location
ARM <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/ARM
ColdFire <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/ColdFire
DSC <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/DSC
E200 <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/E200
RS08 <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/RS08
S12Z <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/S12Z