The goal of this tutorial is to demonstrate how to protect / unprotect actions enable you to change the protection of a sector in the flash device.
To add a protect / unprotect action:
- Select the Protect/Unprotect action from the Add Action drop-down list.
The
Add Protect/Unprotect Action
dialog box appears.
Figure 1. Add Protect / Unprotect Action Dialog Box 
- Select a sector from the Sectors table and click the Add Protect Action button to add a protect operation on the selected sector.
Note: Press CTRL or SHIFT keys for selecting multiple sectors from the Sectors table.
- Click the Add Unprotect Action button to add an unprotect action on the selected sector.
Note: Check the All Device checkbox to add action on full device.
- Click Done.
The
Add Protect/ Unprotect Action
dialog box closes and the added protect or
unprotect actions appear in the
Flash Programmer Actions
table in the
Flash Programmer Task
editor window.
Figure 2. Protect / Unprotect Action