The Target RAM is used by Flash Programmer to download its algorithms.
| Button/Option | Usage |
|---|---|
| Erase / Blank Check | Lets you add erase or blank check actions for flash devices |
| Program / Verify | Lets you add program or verify flash actions for flash devices |
| Checksum | Lets you add checksum actions for flash devices |
| Diagnostics | Lets you add a diagnostics action to the actions table. |
| Dump Flash | Lets you dump a portion of the flash or the entire flash. |
| Protect/Unprotect | Lets you modify the protection of a sector. |
| Secure/Unsecure | Lets you add secure or unsecure actions. |
| Remove Action | Lets you remove a sector, a group of sector, or an entire device from the Flash Programmer Actions table, depending on the flash capabilities. |
| Move Up | Lets you move a selected flash action up in the Flash Programmer Actions table, so that it executes before other actions beneath it in the table. |
| Move Down | Lets you move a selected flash action down in the Flash Programmer Actions table, so that the action executes after other actions above of it in the table execute. |