Note: This procedure assumes that the
Target Tasks view is visible in the perspective. If it is not visible, perform the steps in the
Working with Flash Programmer topic to open the
Target Tasks view.
After you have launched CodeWarrior and the machine has a USB NEXUS Multilink connected to a Leopard (for example, MPC5643L) LSM board:
- Go to the Target Tasks view in either the C/C++ or Debug perspective.
- Right-click on this view and select Import . Alternatively, click the Import icon on the Target Tasks view toolbar.
The
Open
dialog box appears.
- Navigate to <CWInstallDir>/MCU/bin/plugins/support/TargetTask/Flash_Programmer/E200 and select the XML file for the board's microcontroller. For this tutorial, select MPC5643L_LSM_VLE.xml.
- Click Open.
The
MPC5643L_LSM_VLE task appears in the
Target Tasks
view.
- Double-click on the MPC5643L_LSM_VLE to examine its contents.
The <target>
Flash Programmer Task
editor window appears, and displays the
memory settings and actions for the task. Notice the actions to erase the contents of
flash memory in the
Flash Programmer Actions
group. These actions execute in the
order as they are displayed in the table, from top to bottom.
Figure 1. Settings for MPC5643L_LSM_VLE Target Task