Flash Programmer Tutorials

This topic consists of two tutorials that demonstrate how to import and execute pre-defined target tasks. Additionally, there are tutorials on how use the <target> Flash Programmer Task editor window to create tasks, such as erasing on-chip memory, or downloading a file, and writing it into flash memory.

Note: The Flash Programmer for RS08 works only if OSBDM connection is used.

The tutorials include: