Execute Predefined Task

To execute the task:

  1. Right-click on the imported task.
  2. Select Execute . Alternatively, select the imported task and click the Execute icon on the Target Tasks view toolbar.

    CodeWarrior establishes contact with the board, erases the microcontroller's flash memory, downloads the code, and verifies that the contents of flash match those of the file.

Congratulations! You have selected and used a target task that erased and programmed the flash memory on the pre-defined Power Architecture task.