Execute MCF5213_INTFLASH Task

To execute the task:

  1. Right-click on the MCF5213_INTFLASH task.
  2. Select Execute . Alternatively, select the MCF5213_INTFLASH task and click the Execute icon on the Target Tasks view toolbar.

    CodeWarrior establishes contact with the MCF5213-based board board, erases the microcontroller's flash memory, downloads the code, and verifies that the contents of flash match those of the file.

Congratulations! You have selected and used a target task that erased and programmed the flash memory on the MCF5213 microcontroller.