Creating Flash Programmer Target Task

  1. Select Windows > Show Views > Others from the IDE menu bar.

    The Show View dialog box appears.

  2. Expand the Debug group and select Target Tasks.
  3. Click OK.

    The Target Tasks view appears.

  4. Click the Create a new Target Task icon in the Target Tasks view toolbar.

    The Create New Target Task wizard appears.

  5. In the Task Name text box, enter the name of the target task.
  6. From the Run Configuration drop-down list, select a configuration.
    Note: Select Active Debug Context from the Run Configuration drop-down list, if you want to use Flash Programmer over an active debug session, else select any of the specified debug context from the list.
  7. From the Task Type drop-down list, select the appropriate Flash Programmer.
    Figure 1. Create New Target Task Wizard
    Create New Target Task Wizard
  8. Click Finish.

    The <target> Flash Programmer Task editor window appears.

    Note: The <target> Flash Programmer Task editor window has groups to define flash devices, Flash Programmer actions, and target RAM settings.