To add a flash device to the Flash Devices
table:
- Click the Add Device button.
The Add Device
dialog box appears.
Figure 1. Add Device Dialog Box 
- Select a flash device from the device list.
- Click Add Device from the Flash Devices group to add a new hardware device.
The Add Device
dialog box appears with a list of supported devices.
- Select the specific device from the list.
- Change the device's memory organization (if required).
Note: To change the device memory organization, click the adjacent value in the Organization column. Click the down button icon, and select the required organization.
- Click Add Device.
You get a popup with a status that the device is added.
Figure 2. Add Device Dialog Box - Popup with Status 
- You can select other devices, if required.
- Click Done.
The Add Device
dialog box closes. The devices appear in the Flash Devices
group of
the <target> Flash Programmer Task
editor window.