Add Secure/Unsecure Actions

The secure/unsecure actions enable you to change the security of a flash device.

To add a secure/unsecure action:

  1. Select the Secure/Unsecure action from the Add Action drop-down list.

    The Add Secure/UnSecure Action dialog box appears.

  2. Select a device from the Flash Devices table.
  3. Click the Add Secure Action button to add Secure action on the selected flash device.
    1. Type a password in the Password text box.
    2. Select the password format from the Format drop-down list box.
  4. Click the Add Unsecure Action button to add an unprotect action on the selected sector.
  5. Click Done.

    The Add Secure/UnSecure Action dialog box closes and the added secure or unsecure action appears in the Flash Programmer Actions table in the Flash Programmer Task editor window.