Add Protect/Unprotect Actions

The protect/unprotect actions enable you to change the protection of a sector in the flash device.

To add a protect/unprotect action:

  1. Select the Protect/Unprotect action from the Add Action drop-down list.

    The Add Protect/Unprotect Action dialog box appears.

  2. Select a sector from the Sectors table and click the Add Protect Action button to add a protect operation on the selected sector.
    Note: Press CTRL or SHIFT keys for selecting multiple sectors from the Sectors table.
  3. Click the Add Unprotect Action button to add an unprotect action on the selected sector.
  4. Check the All Device check box to add action on full device.
  5. Click Done.

    The Add Protect/Unprotect Action dialog box closes and the added protect or unprotect actions appear in the Flash Programmer Actions table in the Flash Programmer Task editor window.