In the
Flash Programmer Actions
group in the Flash Programmer Task editor window, add the flash programmer actions to be performed on the flash device. You can perform
the following actions on a flash device.
Note: Actions can also be enabled or disabled using the Enabled column. The Description column contains the default description for the flash programmer actions. You can also edit the default description.