The diagnostics action generates the diagnostic information for a selected flash device.
Note: Flash Programmer will report bad blocks, if they are present in the NAND flash.
To add a diagnostics action:
- Select the Diagnostics action from the Add Action drop-down list.
The
Add Diagnostics
dialog box appears.
- Select a device to perform the diagnostics action.
- Click the Add Diagnostics Action button to add diagnostic action on the selected flash device.
Note: Check the Perform Full Diagnostics check box to perform full diagnostics on a flash device.
- Click Done.
The
Add Diagnostics Action
dialog box closes and the added diagnostics action
appears in the
Flash Programmer Actions
table in the
Flash Programmer Task
editor window.