P&E USB Multilink Universal [FX]/USB Multilink

The P&E S12Z Connection setting permits a connection to USB Multilink devices, which include the P&E BDM Multilink, USB Multilink Universal, and the USB Multilink Universal FX. The P&E USB Multilink Universal [FX]/USB Multilink mode lets you debug code, as the firmware is fully resident in the Flash of the microprocessor. The operation of all modules fully reflects the actual operation of the onboard resources. Like the USB Multilink Universal, the USB Multilink Universal FX can conveniently debug all Freescale architectures found in the current CodeWarrior 10 version, however, the FX version is up to 8 times faster than the USB Multilink Universal and it can also provide power to the target.