The P&E Connection Assistant is displayed when you attempt to debug but CodeWarrior
cannot connect to the interface hardware specified in the Launch Configuration dialog
box. To edit or change your debugger connection:
1. Choose the P&E device that you are using from
- Choose the P&E device that you are using from the first drop-down menu and click Refresh.
- Using the second drop-down menu, select the port on which the interface is connected.
- Use the BDM Communication Speed panel to configure the shift frequency and delay.
- Click the Retry button.