Active Mode Menu Options

When the microprocessor is connected, the active mode menu shows the name of the microprocessor and gives you the access to P&E Microcomputer Systems' Compatible Hardware Interfaces web page and home page. If the OSBDM interface is being used for the debugging session, then the OSBDM Documentation option appears within the active mode menu, which takes you to P&E Microcomputer Systems' OSBDM website. When the microprocessor is not connected, the menu is not available.

Figure 1. Additional Connection Menu Options
Additional Connection Menu Options