P&E TraceLink Ethernet

The P&E TraceLink Ethernet Connection setting permits a connection to TraceLink Ethernet devices. P&E TraceLink Ethernet mode lets you debug code, as the firmware is fully resident in the Flash of the microprocessor. The operation of all modules fully reflects the actual operation of the onboard resources. P&E's TraceLink can conveniently support all Freescale architectures found in the current CodeWarrior 10 version; however, it can only capture the external trace signals for the ColdFire V2/3/4 and Kinetis ARM architectures.

Note: For external trace captures, the P&E TraceLink supports ETM trace. The Kinetis chip must have the Trace_CLKOUT and Trace_D[3:0] pins to support ETM trace. Chips without these pins can still be debugged by the TraceLink within CodeWarrior.