Connection Assistant

The P&E Connection Assistant is displayed when you attempt to debug but CodeWarrior cannot connect to the interface hardware specified in the Launch Configuration dialog box. To select the P&E Multilink/Cyclone /OSBDM as your debugger connection::

  1. Select the P&E device that you are using from the first drop-down menu and click Refresh.
  2. Using the second drop-down menu, select the port on which the interface is connected.
  3. Use the Cyclone Power Control panel to configure the power and delay settings (Cyclone only).
  4. Click the Retry button.