Connections - ColdFire V1/ColdFire+ V1

This chapter describes the features and settings of the connections that interface the CodeWarrior debugger with the ColdFire V1/ColdFire+ V1 target board.

For the IDE to communicate with the target hardware, you must specify several key items: the debugger protocol, a connection type, and any connection parameters. You can enter these items using options in the Launch Configuration panel. Launch Configuration panel can be accessed by clicking on the Edit button located within the Main tab of the Debug Configurations dialog box. These options are:

The topics in this chapter discuss the features and settings of the connections that interface the CodeWarrior debugger with the ColdFire V1/ColdFire+ V1 device family.

Note: The MMA95xx sensor chip uses the ColdFire V1 chip core; therefore, users should use the ColdFire V1/ColdFire+ V1 connection settings within the CodeWarrior debugger.