SPDO Command

The SPDO command displays the output buffer from the SPI. A window opens that shows all the data that the SPI has shifted out. An arrow points to the last output value transmitted. The maximum number of output values that the buffer holds is 256 bytes.

Syntax
  >gdi SPDO  
Example
  >gdi SPDO  

View data from the output buffer for the SPI simulation.

Figure 1. SPI OUT Buffer Display
SPI OUT Buffer Display