Modulo Timer Interrupt Module

In Full Chip Simulation (FCS) mode, this module simulates all functionality of the Modulo Timer Interrupt (MTIM) Module, including:

Once the MTIM Status and Control register properly configures the operation of the module, the MTIM Counter starts incrementing. If modulo up count operation is enabled, you can observe the MTIM overflow flag in the MTIM Status and Control register in the Memory window.

Figure 1. Memory Component Window
Memory Component Window

If the MTIM interrupt is enabled, the FCS jumps to an appropriate subroutine as long as the MTIM interrupt vector is properly defined.