All connection settings for P&E hardware interfaces are configured using the Connection group in the Main tab of the Debugger Configuration dialog box.
The following table describes the options for this view.
| Option | Description |
|---|---|
| Interface | Use this option to select the interface type. Select a supported interface from the list box. The options are:
|
| Refresh | Click this button to have the workstation scan for a valid interface and port. Valid interfaces and ports appear in the Interface and Port list boxes. |
| Port | This option selects the port over which debug communications is conducted. Select an available port from the list box. NOTE: If you are having issues trying to get a port to display, click on the [FAQ #29] link for help. |
| Socket Programming Options | The Socket Programming Options button brings up a dialog that provides you with a graphical representation of the signals that must be connected from the BDM header to the pins of the microprocessor, in order to use Freescale socket adapters. |
| Advanced Programming Options | The Advanced Programming Options button brings up a dialog that provides you with options to configure the flash programming procedure. |
| Specify IP (Cyclone Ethernet only) | Use this option to specify the IP address of a Cyclone outside of the local network. Click on the checkbox to enable the textbox. This will also disable the port dropdown box. Currently supports IPv4 only. |
| Specify Network Card IP (Cyclone Ethernet only) | Use this option to specify the local network card IP address if there are multiple cards on your computer. Click on the checkbox to enable the textbox. Currently supports IPv4 only. |
| Provide power to target (Cyclone and USB Multilink Universal FX only) | Check this option to have the Cyclone or USB Multilink Universal FX (circuitry) supply power to the hardware target. Uncheck this option to not provide power. Note: For USB Multilink Universal FX, use the jumper settings located at JP10 to provide either 3.3V or 5V.
|
| Power off target upon software exit (Cyclone and USB Multilink Universal FX only) | Check this option to turn off the power when the program terminates. Uncheck this option to leave the hardware target powered continuously. |
| Regulator Output Voltage (Cyclone and USB Multilink Universal FX only) | This option adjusts the output voltage that powers the hardware target. Select a voltage value from this option's list box. |
| Power down delay (Cyclone and USB Multilink Universal FX only) | This option specifies amount of time for which the target will be turned off during a RESET power cycling sequence. Enter the delay interval (in milliseconds) in this option's text box. |
| Power up delay (Cyclone and USB Multilink Universal FX only) | This option specifies amount of time for which the target will remain powered prior to a RESET power cycling sequence. Enter the delay interval (in milliseconds) in this option's text box. |
To change P&E Connections settings, perform these steps.
The Debug Configurations dialog box appears.
The Main page appears in the area beneath the tabs.
Valid interfaces and ports appear in the Interface and Port drop-down lists in the Connection Port and Interface Type group.