PR<x>INPUT<y> Command

The PR<x>INPUT<y> command allows the user to input voltage value for the external analog input CIN<y>. For HCS08 devices that have more than one PRACMP module, <x> is the number representing the corresponding module. For HCS08 devices that only have one PRACMP module, <x>=1.

Syntax
  >gdi PR<x>INPUT<y> <n>  

Where: <x> is the number representing the corresponding PRACMP module

<y> is the number representing the corresponding external analog input CIN

<n> is the voltage input value

Examples
  >gdi PR1INPUT1 5.00  

Simulate the input 5.00 volts on CIN1 of PRACMP1.

  >gdi PR4INPUT3 2.50  

Simulate the input 2.50 volts on CIN3 of PRACMP4.