PR<x>INPUTS Command

In FCS Mode, the PR<x>INPUTS command opens the PRACMP<x> Input Value dialog box shown in the following figure. The user may then use this box to specify the external analog input voltages. For HCS08 devices that have more than one PRACMP module, <x> is the number representing the corresponding module. For HCS08 devices that only have one PRACMP module, <x>=1.

Figure 1. PRACMPx Input Value dialog box
PRACMPx Input Value dialog box

When using FCS, the PR<x>INPUTS command shows the simulated input analog voltages to any applicable PRACMPx module.

Syntax
  >gdi PR<x>INPUTS  

Where: <x> is the number representing the corresponding PRACMP module

Example
  >gdi PR1INPUTS  

Show input analog voltages of PRACMP1.