PGAINVDDA <x> Command

The PGAINVDDA <x> command allows the user to input a value for the VDDA signal that the PGA module connects to.

Syntax
  >gdi PGAINVDDA <x>  

Where: <x> is the input value in volts

Examples
  >gdi PGAINVDDA 1.50  

Simulate the input 1.50 volts for VDDA signal