Keyboard Interrupt Module

In Full Chip Simulation (FCS) mode, this module simulates all functionality of the Keyboard Interrupt (KBI) module, including the edge-only, edge and level interrupt, and flag polling modes of operation. FCS mode uses simulated port inputs to trigger the KBI event from the proper I/O port pin.

To define an input state of the specific port, write the INPUT<x> <n> command in the Command window. The <x> represents the corresponding I/O port, while <n> stands for the input value to write to this port. At the same time, you can use the INPUTS command to bring up the Simulated Port Inputs for all general I/O ports. It displays the current simulated values to all applicable input ports. Refer the documentation for Timer Module Commands for more information about the various forms of this command.

Figure 1. Simulated Port Inputs Dialog Box
Simulated Port Inputs Dialog Box

Use the Simulated Port Inputs dialog box to reconfigure the input value to any I/O port. To trigger the event, manipulate the inputs to the port in the appropriate manner, depending on whether the KBI is configured for edge-only or edge and level. Once the KBI event takes place, you can observe the KEYF Flag bit, which is a part of the Keyboard Status and Control register, in the Memory window.

Figure 2. Memory Component Window
Memory Component Window

You can poll the KBI Interrupt Pending flag if the Polling Mode is simulated. In Interrupt Mode, the simulator branches to an appropriate interrupt subroutine as long as the KBI interrupt vector is properly configured.

Note: For more information on KBI configuration, refer to the Freescale user manual for your microprocessor.