In Full Chip Simulation (FCS) mode, this module simulates all input and output functionality of the Input/Output (I/O) Ports module. FCS mode uses a set of designated commands to simulate the input and output activity on corresponding I/O port pins. To define an input state of a specific port, write the INPUT <x> <n> command in the Command window. The <x> represents the corresponding I/O port, while the <n> stands for the input value to write to this port. At the same time, you can use the INPUTS command to bring up the Simulated Port Inputs for all general I/O ports. It displays the current simulated values to all applicable input ports.
Use the Simulated Port Inputs dialog box to reconfigure the input value to any I/O port. Use the INPUTS command to reconfigure the output values on any relevant I/O port. You can observe the manipulation of I/O port pins in the Memory window.
Note that if the regular I/O pins are multiplexed to be used by a different MCU Module, they might not be available for general I/O functionality.