In FCS mode, the HSC<x>INPUTS command opens the HSCMP<x> Input Value dialog box shown in the following figure. The user may then use this box to specify the external analog input voltages. For HCS08 devices that have more than one HSCMP module, <x> is the number representing the corresponding module. For HCS08 devices that only have one HSCMP module, <x>=1.
When using FCS, the HSC<x>INPUTS command shows the simulated input analog voltages to any applicable HSCMPx module.
>gdi HSC<x>INPUTS
Where:
<x> is the number representing the corresponding HSCMP module
>gdi HSC1INPUTS
Show input analog voltages.