Connection Assistant

The P&E Connection Assistant is displayed when you attempt to debug and the program cannot connect to the interface hardware specified in the Launch Configuration dialog box. To edit or change your debugger connection:

  1. Select the P&E device that you are using from the first drop-down list and click Refresh..
  2. Using the second drop-down list, select the port on which the interface is connected.
  3. Use the Cyclone Power Control panel to configure the power and delay settings (Cyclone only).
  4. Click the Retry button.