The ADDID command allows the user to input the differential data into the ADC16 converter. A window is displayed that allows the user to input differential values. The user may specify the differential data of the Differential Analog Channel (DADx) input voltages, the Temperature Sensor (TEMP) input, and the Voltage References (VREF).
Figure 1. ADC Differential Data Display 
When using FCS, the ADDID command shows the simulated differential inputs to the ADC16 module.
Syntax
>gdi ADDID
Example
>gdi ADDID
Pull up the differential data window