Connections - HCS08 Architecture

This chapter describes the features and settings of the connections that interface the CodeWarrior debugger with the HCS08 simulator or the target board.

For the IDE to communicate with the target hardware, you must specify several key items: the debugger protocol, a connection type, and any connection parameters. You can enter these items using options in the Launch Configuration panel. The Launch Configuration panel can be accessed by clicking on the Edit button located within the Main tab of the Debug Configurations dialog box. These options are:

The topics in this chapter discuss the features and settings of the connections that interface the CodeWarrior debugger with simulation platforms and hardware devices that are part of the HCS08 device family.

The topics in this chapter are: