cmdwin::eppc::setcoreid

Set the core ID.

Syntax

  cmdwin::eppc::setcoreid  <coreID>  

Examples

The table below lists and defines the examples of the cmdwin::eppc::setcoreid command.

Table 1. cmdwin::eppc::setcoreid Command-Line Debugger Command - Examples
Command Description
cmdwin::eppc::setcoreid 1 Set the core ID value to 1.
cmdwin::eppc::setcoreid default Set the core ID value to default. All commands will be executed on the new set core. To see the current core ID use getcoreid command.