Use this panel to specify the settings for disabling the user messages for the S12Z Linker to use.
The following table lists and describes the disable user messages options for S12Z Linker.
| Option | Description |
|---|---|
| Disable all Messages | Use this option to disable all user messages. This option disables messages that are not in the normal message categories like, WARNING, INFORMATION, ERROR, or FATAL by reducing the amount of messages, and simplifying the error parsing of other tools. |
| Display Type of Messages | Use this option to disable the type of messages. |
| Disable Informal Messages (e.g. memory model, floating point format) | Use this option to disable the informal messages (e.g., memory model, floating point format). |
| Disable Included Files Messages | Use this option to disable the messages about the generated files. |
| Disable Reading Files Messages (e.g. input files) | Use this option to disable the messages about the reading files. |
| Disable Generated Files Messages | Use this option to disable the messages about the include files. |
| Disable Processing Statistics Messages (e.g. code size, RAM/ROM usage) | Use this option to disable the messages about processing statistics. |