Use this panel to specify the host settings of the S12Z.
The following table lists and describes the memory model options for S12Z.
| Option | Description |
|---|---|
| Borrow License Feature | This option allows you to borrow a license feature until a given date or time. Borrowing allows you to use a floating license even if disconnected from the floating license server. |
| Wait Until a License is Available from Floating License Server | By default, if a license is not available from the floating license server, then the application will immediately return. With -LicWait set, the application will wait (blocking) until a license is available from the floating license server. |
| Application Standard Occurrence | This option allows you to select the way you want the application window to start. Normally, the application starts with a normal window if no arguments are given. If you start the application with arguments (e.g., from the Maker to assemble, compile, or link a file), then the application runs minimized to allow for batch processing. However, you may specify the application's window behavior with the View option.
|
| Set Environment Variable | This option sets an environment variable. Use this environment variable in the maker, or use to overwrite system environment variables. |
The following table lists and describes the toolbar buttons for the Set Environment Variable option.
| Button | Description |
|---|---|
| Add - Click to open the Enter Value dialog box and specify the object file search path. | |
| Delete - Click to delete the selected object file search path. | |
| Edit - Click to open the Edit Dialog dialog box and update the selected object file search path. | |
| Move up - Click to move the selected object file search path one position higher in the list. | |
| Move down - Click to move the selected object file search path one position lower in the list. |
The following figure shows the Enter Value dialog box for the Set Environment Variable option in the S12Z Linker > Host panel.
The following figure shows the Edit Dialog dialog box for the Set Environment Variable option in the S12Z Linker > Host panel.
The buttons in the Enter Value and Edit Dialog dialog boxes help work with the object file search paths.