Use this panel to specify disassembler input settings.
The following table lists and describes the disassembler input settings options for S12Z.
| Option | Description |
|---|---|
| Object File Format | Use this option to specify the object file format. The options available are:
|
| Set processor | Specifies which processor should be decoded. For object files, libraries and applications, the processor is usually detected automatically. For S-Record and Intel Hex files, however, the decoder cannot determine which CPU the code is for, and therefore the processor must be specified with this option to get a disassembly output. Without this option, only the structure of a SRecord file is decoded. |