S12Z Disassembler > Host

Use this panel to specify the host settings of the S12Z disassembler.

The following table lists and describes the host options for S12Z.

Table 1. Tool Settings - S12Z Disassembler > Host
Option Description
Borrow License Feature This option allows you to borrow a license feature until a given date or time. Borrowing allows you to use a floating license even if disconnected from the floating license server.
Wait Until a License is Available from Floating License Server By default, if a license is not available from the floating license server, then the application will immediately return. With -LicWait set, the application will wait (blocking) until a license is available from the floating license server.
Application Standard Occurrence This option allows you to select the way you want the application window to start. Normally, the application starts with a normal window if no arguments are given. If you start the application with arguments (e.g., from the Maker to assemble, compile, or link a file), then the application runs minimized to allow for batch processing. However, you may specify the application's window behavior with the View option.
  • -ViewWindow, the application appears with its normal window.
  • -ViewMin, the application appears as an icon in the task bar.
  • -ViewMax, the application appears maximized (filling the whole screen).
  • -ViewHidden, the application processes arguments (e.g., files to be compiled or linked) in the background (no window or icon visible in the task bar).
Set Environment Variable This option sets an environment variable. Use this environment variable in the maker, or use to overwrite system environment variables.

The following table lists and describes the toolbar buttons for the Set Environment Variable option.

Table 2. Toolbar Buttons - Set Environment Variable Option
Button Description
Add - Click to open the Enter Value dialog box and specify the object file search path.
Delete - Click to delete the selected object file search path.
Edit - Click to open the Edit Dialog dialog box and update the selected object file search path.
Move up - Click to move the selected object file search path one position higher in the list.
Move down - Click to move the selected object file search path one position lower in the list.

The following figure shows the Enter Value dialog box for the Set Environment Variable option in the S12Z Disassembler > Host panel.

Figure 1. Set Environment Variable - Enter Value Dialog Box
Set Environment Variable - Enter Value Dialog Box

The following figure shows the Edit Dialog dialog box for the Set Environment Variable option in the S12Z Disassembler > Host panel.

Figure 2. Set Environment Variable - Edit Dialog
Set Environment Variable - Edit Dialog

The buttons in the Enter Value and Edit Dialog dialog boxes help work with the object file search paths.