S12Z Disassembler

Use this panel to specify the command, options, and expert settings for S12Z Disassembler.

The following table lists and describes the disassembler options for S12Z.

Table 1. Tool Settings - DSC Disassembler
Option Description
Command Shows the location of the preprocessor executable file. Default value is "${S12Z_ToolsDir}/decoder". You can specify additional command line options for the preprocessor; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the linker will be called with.
Expert settings
Command line pattern Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}