S12Z Compiler > Access Paths

Use this panel to specify access path options for the S12Z Compiler.

The following table lists and describes the access paths options for S12Z.

Table 1. Tool Settings - HCS08 Compiler > Language Options
Option Description
Do Not use MWCIncludes Variable This option inhibits the usage of MWCInclude variables. By default, this checkbox is checked.
Always Search User Paths Use this option to enable the usage of the search paths.
Search User Paths (#include "...") Use this option to specify the user paths.
Search User Paths Recursively Use this option to specify the user paths recursively.
Search System Paths (#include <...>) Use this option to specify the system paths.
Search System Paths Recursively Use this option to specify the system paths recursively.

The following table lists and describes the toolbar buttons that help work with the libraries and the additional object file search paths.

Table 2. Search Paths Toolbar Buttons
Button Description
Add - Click to open the Add directory path dialog box and specify the object file search path.
Delete - Click to delete the selected object file search path.
Edit - Click to open the Edit directory path dialog box and update the selected object file search path.
Move up - Click to move the selected object file search path one position higher in the list.
Move down - Click to move the selected object file search path one position lower in the list.

The following figure shows the Add directory path dialog box.

Figure 1. Add directory path Dialog Box
Add directory path Dialog Box

The following figure shows the Edit directory path dialog box.

Figure 2. Edit directory path Dialog Box
Edit directory path Dialog Box

The buttons in the Add directory path and Edit directory path dialog boxes help work with the object file search paths.