Use this panel to control how the burner generates the output file, as well as error and warning messages. You can specify whether to allocate constant objects in ROM, generate debugging information, and strip file path information.
Use this panel to configure the S-record options of the Burner.
The following table lists and describes the general options for S12Z configure S-Record panel.
| Option | Description |
|---|---|
| Select all | This option disables the generation of all records, from the start (S0) to the end records (S7, S8, or S9). |
| No path in S0-record | This option removes the path (if present) from the file name in the S0 record. |
| No S9-record | This option disables the generation of S9-record. |
| No S8-record | This option disables the generation of S8-record. |
| No S7-record | This option disables the generation of S7-record. |
| No S0-record | This option disables the generation of S0-record. |