Use the Burner for S12Z Preference Panel to select the settings for the S12Z Burner.
The following table lists and describes the burner options for S12Z.
| Option | Description |
|---|---|
| Command | Shows the location of the burner executable file. Default value is: "${S12Z_ToolsDir}/burner". You can specify additional command line options for the burner; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the burner will be called with. |
| Expert Settings | Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${INPUTS}. |
| Command line pattern |