S12Z Assembler > Input

Use this panel to specify the input settings for S12Z assembler.

The following table lists and describes the input options for S12Z.

Table 1. Tool Settings - S12Z Assembler > Input
Option Description
Case Insensitivity on Label Name Use this option to enable the case insensitivity on the label name.
Define Label (use spaces to separate labels) Use this option to specify the label names.
Support for Structured Types This option enables the support for the structured types.
Include File Search Path Use this option to specify the include file search path.

The following table lists and describes the toolbar buttons that help work with the libraries and the additional object file search paths.

Table 2. Search Paths Toolbar Buttons
Button Description
Add - Click to open the Add directory path dialog box and specify the object file search path.
Delete - Click to delete the selected object file search path.
Edit - Click to open the Edit directory path dialog box and update the selected object file search path.
Move up - Click to move the selected object file search path one position higher in the list.
Move down - Click to move the selected object file search path one position lower in the list.

The following figure shows the Add directory path dialog box.

Figure 1. Add directory path Dialog Box
Add directory path Dialog Box

The following figure shows the Edit directory path dialog box.

Figure 2. Edit directory path Dialog Box
Edit directory path Dialog Box

The buttons in the Add directory path and Edit directory path dialog boxes help work with the object file search paths.