S12Z Assembler > General

Use this panel to specify the general assembler behavior.

The following table lists and describes the general assembler options for S12Z.

Table 1. Tool Settings - Assembler > General Options
Option Description
MCUasm Compatibility Check to activate the compatibility mode with the MCUasm Assembler.
Other Flags Specify additional command line options for the assembler; type in custom flags that are not otherwise available in the UI.