RS08 Compiler > Optimization > Optimize Library Function

This option enables the compiler to optimize specific known library functions to reduce execution time. The Compiler frequently uses small functions such as strcpy(), strcmp(), and so forth. Use this panel to configure the optimize library function options for the RS08 compiler.

The following table lists and describes the Mid level branch optimizations options for RS08 compiler.

Table 1. Tool Settings - RS08 Compiler > Optimization > Mid level branch optimizations
Option Description
Apply all optimizations (-OiLib) This option applies all the optimizations.
shifts left of 1 (-OiLib=g) This option replace shifts left of 1 by array lookup.
memcpy (-OiLib=f) This option inline calls to the memcpy() function.
memset (-OiLib=e) This option inline calls to the memset() function.
fabs/fabsf (-OiLib=d) This option inline calls to the fabs() or fabsf() functions.
strlen (-OiLib=b) This option inline calls to the strlen() function.