Use this panel to specify the command, options, and expert settings for the build tool compiler. Additionally, the RS08 Compiler tree control includes the general and the file search path settings.
| Option | Description |
|---|---|
| Command | Shows the location of the compiler executable file. Default value is : " ${HC08Tools}/crs08.exe". You can specify additional command line options for the compiler; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the compiler will be called with. |
| Expert Settings | |
| Command line pattern | Shows the command line pattern; default is {COMMAND} ${FLAGS}${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}. |