Use this panel to specify preprocessor behavior and define macros.
The following table lists and describes the preprocessor options for PowerPC.
| Option | Description |
|---|---|
| Command | Shows the location of the preprocessor executable file. Default value is "${PAToolsDir}/mwcceppc". You can specify additional command line options for the preprocessor; type in custom flags that are not otherwise available in the UI. |
| All options | Shows the actual command line the linker will be called with. |
| Expert settings Command line pattern | Shows the command line pattern; default is ${COMMAND} ${FLAGS} ${OUTPUT_FLAG} ${INPUTS} |