PowerPC Disassembler

Use this panel to specify the command, options, and expert settings for PowerPC Disassembler.

The following table lists and describes the PowerPC disassembler options.

Table 1. Tool Settings - PowerPC Disassembler
Option Description
Command Shows the location of the disassembler executable file. Default value is powerpc-linux-gnu-as. You can specify additional command line options for the disassembler; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the linker will be called with.
Expert settings
Command line pattern Shows the command line pattern; default is "${PAGCCINSTALLDIR}/${COMMAND}" ${FLAGS} ${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT}${INPUTS}