Use this panel to specify the code generation assembler behavior.
The following table lists and describes the code generation assembler options for HCS08.
| Option | Description |
|---|---|
| Associate debug information to assembly source file (-AsmDbg) | Passes the assembly source file name information to DWARF sections. When the output .abs file is debugged, the actual assembly source file is displayed instead of intermediary <filename>.dbg file. |