DSC Linker > Output

Use this panel to specify the output settings for the DSC linker output.

The following table lists and describes the linker options for DSC.

Table 1. Tools Settings > DSC Linker > Output
Option Description
Output Type Select output type as Application (default) or Library.
Generate Link Map Check to generate link map.
List Unused Symbols in Map Check to list unused symbols; appears grayed out if the Generate Link Map checkbox is not checked.
Show Transitive Closure in Map Check show transitive closure; appears grayed out if the Generate Link Map checkbox is not checked.
Annotate Byte Symbols in Map Checked - Linker includes B annotation for byte data types (e.g., char) in the Linker Command File. Clear - By default, the Linker does not include the B annotation in the Linker Command File. Everything without the B annotation is a word address.
Generate ELF Symbol Table Check to generated the ELF symbol table.
Generate S-Record File Check to generate a S-record file.
Sort by Address Check to sort by address.
Generate Byte Addresses Check to generate byte address.
Max S-Record Length Specify the maximum length for S-record; appears grayed out if the Generate S-Record File checkbox is not checked. The default value is 252.
S_Record EOL Character Specify the end-of-line character; appears grayed out if the Generate S-Record File checkbox is not checked. The default value is DOS (\r\n).